NORD ELECTRONIC DRIVESYSTEMS - Aurich

alt

Electronics production

Since the early 1980s, NORD DRIVESYSTEMS, one of the world's leading full-range suppliers of electrical, mechanical and electronic drive technology, has had its own electronics production facility in the north-west of Lower Saxony. Every NORD frequency inverter – whether it is operated in Europe, China or the US, and whether it is a control cabinet inverter or decentralised frequency inverter – is produced in the NORD production plant in Aurich.

Over the years, we have been continuously expanding both our portfolio and the site. Today, we employ around 200 people at the local NORD Electronic DRIVESYSTEMS GmbH (plus another 40 engineers in product development at the headquarters in Bargteheide) and produced 185,000 units in 2022, and the trend increases. The production area is 7,000 m2 and the office area 1,300 m2. The range includes electronic drive technology up to 160 kW (inverters, motor starters and electronics).

Continuous investment

Continuous investments are being made in the Aurich location and capacities are being further expanded. Around EUR 2.5 million have recently been invested in the expansion, which has increased the assembly area to 3,000 m2. The maximum production capacity is now at 400,000 units, i.e. frequency inverters of all types. The purchase of an adjacent site with an area of 1.8 ha secures further expansion. Planning for the production expansion is already underway.

Lean logistics – efficient processes

The automated and flexible production structure in Aurich is state-of-the-art and allows any size of order to be processed. Even small batch sizes are possible thanks to flexible production. The products are manufactured directly on customer order. They are configured in SAP at the final assembly level and then fitted and assembled to the customer's request.

A central order controls the entire production. All data and information are combined online and can be accessed from anywhere at all times. Among other things, placement and test plans are automatically generated from the individual configuration, both in THT production (through hole technology) and in the SMD area (surface mounted device).

An automated guided vehicle system (AGV) also ensures greater efficiency. Among other things it is responsible for the transport from goods receipt to the automated small parts warehouse.

The efficient process begins as early as at goods receipt. Each package is given a 2D code so that it can be fully tracked until it is used, or inversely from the serial number of the device back to the goods receipt (traceability).

Aurich job offers

Support us in manufacturing

Are you interested in a career in gear unit manufacturing? In the job overview you can find our job offers in Aurich in manufacturing as well as other offers in other areas and locations. Apply simply and directly by e-mail.

Job offers

From printed circuit board to finished product

In SMD production, the two assembly lines place as many as 70,000 electronic components per hour. In order to ensure fault-free production, all modules are checked using an in-line AOI system (automatic optical inspection) after placement and soldering in a nitrogen atmosphere.

In THT production, the wired components are assembled and soldered with wave soldering systems in a nitrogen atmosphere. Depending on the complexity, a THT AOI test and a subsequent 100% function test are carried out. From THT production, the modules are conveyed to a final assembly Kanban warehouse. In the different assembly areas, the devices are then assembled on semi-automatic lines.

Eliminating sources of error, maintaining quality standards

The frequency inverters must meet high quality standards prior to delivery. To maintain this, appropriate quality controls are integrated in Aurich at all production stages. This starts with component checks in goods receipt and continues with the upgrading of the automatic placement machines.

The AOI test in SMD and THT is set up in such a way that even the slightest deviations are registered. After THT production, all modules are tested electrically once again. During the final testing of the devices, the final performance test is carried out under full load.

Digitalisation, automation and maximum flexibility

The test systems are optimally matched to the testing requirements – many systems, both hardware and software, were developed by in-house test equipment manufacturing. This ensures additional safety – as do the visualisation of the assembly instructions and the laser marking of the devices. This is the only way of guaranteeing the high quality and reliability of NORD products.

“Manufacturing the NORDAC frequency inverter in Aurich demonstrates: We do not compromise at NORD DRIVESYSTEMS when it comes to our own manufacturing process. Digitalisation, automation and maximum flexibility have long since found their way into the factory halls”, plant manager Gerhard Harms emphasises.

Find out more about NORD drive technology

Drive electronics

NORD DRIVESYSTEMS provides intelligent solutions with electronic drive technology for demanding applications. NORD supplies frequency inverters and motor starters both as decentralised and control cabinet installation variants. Our NORD applications team will be glad to assist you in the selection of the optimal drive system.

How a frequency inverter is built: A look behind the scenes in Aurich

The age of industrial mass production with only a few product versions and large quantities is long gone. Individuality is in greater demand than ever. Customers increasingly demand specific configurations which are precisely tailored to their individual requirements. This megatrend will continue in the future.

How to find us

NORD Electronic Drivesystems
Tjüchkampstraße 37
D-26605 Aurich‎
Niedersachsen

From Hamburg

Drive around 100 km on the A1 towards Bremen. At the interchange 58a-Dreieck Stuhr take the exit to merge onto the A28 towards Oldenburg/Delmenhorst/Stuhr/Groß-Mackenstedt. After around 42 km, at the interchange 11-Dreieck Oldenburg-West take the exit to stay on the A28 towards Groningen/Emden/Leer/Bad Zwischenahn/Oldenburg-Wechloy. After around 45 km, take the exit 3-Filsum and then turn right to get onto the B72 towards Aurich/Hesel. Follow the B72 for around 6 km and then turn right to stay on the B72 (B436). Follow the B72 for around 18 km and then turn right into Tjüchkampstraße. After around 200 m you have reached your destination.

From the Ruhr area (A31)

Take the A31 northbound (towards Emden/Dorsten). Stay on the A31 for around 200 km until the interchange 9-Dreieck Leer. Take the exit towards Norddeich/Emden/Veenhusen (A31). After around 6 km, take the exit 7-Neermoor and turn right onto the L14/Osterstraße towards Aurich/Timmel. Stay on the road for the next 9 km and then turn left to stay on the L14. Follow the road for another 7 km, cross the B72 and continue straight ahead into Tjüchkampstraße. After around 200 m you have reached your destination.

From Groningen after passing the German border

Coming from the A7 (Netherlands), you are passing the German border. Continue onto the A280. After around 4 km, at the interchange 3-Dreieck Bunde take the exit onto the A31 towards Emden/Leer/Oldenburg/Weener. Stay on the A31 for around 20 km until the interchange 9-Dreieck Leer. Take the exit towards Norddeich/Emden/Veenhusen (A31). After around 6 km, take the exit 7-Neermoor and turn right onto the L14/Osterstraße towards Aurich/Timmel. Stay on the road for the next 9 km and then turn left to stay on the L14. Follow the road for another 7 km, cross the B72 and continue straight ahead into Tjüchkampstraße. After around 200 m you have reached your destination.