NORD SERV

release 5.10.04

This software now works under Windows 95, 98, 2000 and XP.

  1. Download the below file, and unzip the file using Winzip or an other unzip tool.
  2. Run the Setup program from the folder DISK1 and follow the instructions.
  3. Please find in the readme file, which you will find at the end of the installation, the changes from the newest release.

download

NORD SERV 5.10.04 Download | ZIP (4 MB)

The configuration software for the Servo Controller SK 1000E with integrated SPS.

System requirements:

IBM or compatible PC, Pentium or similar processor 32 Megabyte RAM Windows 95, 98, 2000, ME, XP 15 MB free hard disk space, super VGA graphic ( 800x600 ), mouse.

Disclaimer

Getriebebau NORD is not liable for damages resulting form the use of this software, even if Getriebebau NORD has been informed about the possibility of such damages.