News –
NORD DRIVESYSTEMS at the FMB Süd 2022
NORD will be presenting its drive systems at the Mechanical Engineering Fair in Augsburg on 11 and 12 May 2022.
Bargteheide, 2022-04-27
At FMB Süd on 11 and 12 May 2022, the mechanical and plant manufacturers will meet with their suppliers. As one of the leading international full-range suppliers of drive technology, NORD will also be in Augsburg to present its innovative drive systems.
One of the highlights at the NORD stand is the new DuoDrive. The innovative and patented geared motor integrates a high efficiency IE5+ synchronous motor into the housing of a single stage helical gear unit and sets new standards for performance, installation space and reduction of variants. Elimination of many wearing parts results in lower maintenance. Overall, the DuoDrive enables a significant decrease of the Total Cost of Ownership (TCO) in comparison with existing drive systems.
High efficiency, compact design
The energy-efficient IE5+ permanent magnet synchronous motors achieve their high efficiency via a wide torque range – and are optimally suitable for operation in the partial load range for example in intralogistics, the food or pharmaceutical industry. The decentralised frequency inverter NORDAC <i>ON</i> features an integrated Ethernet interface, full plug-in capability and an extremely compact design and offers an economical plug-and-play solution for IIoT environments.
NORD DRIVESYSTEMS will be presenting these and other drive systems on 11 and 12 May 2022 at FMB Süd in Augsburg. You will find the company in Hall 1 at Stand D9.