News –

NORD at SPS in Nuremberg

Successful presentation of the drive specialist at the automation trade fair

Bargteheide, 2024-01-09

The SPS – smart production solutions 2023 trade fair in Nuremberg ended with a significant increase in visitor numbers compared with the previous year. NORD, too, draws a very positive conclusion to the event. “We had inspiring discussions with many customers and prospects, and made valuable contacts”, Jörg Niermann, Head of Marketing at NORD, points out.

The following was presented at the NORD stand:

  • The decentralised NORDAC ON frequency inverters. The NORDAC ON+ version that has been specially optimised for the combination with the IE5+ synchronous motor attracted particular interest.
  • The NORD ECO consulting service, which helps to find a particularly efficient drive solution for individual applications
  • Drive solutions for the end-of-line packaging , which operate particularly economically by using controlled asynchronous drive systems with decentralised frequency inverters
  • The NORDAC PRO control cabinet inverters for powers of up to 37 kW, which provide a large variety of interfaces and functions
  • The NORD sustainability programme , with which the company commits itself to act in an ecologically, economically and socially responsible manner

Requirements and pain points at first hand

There was also an intensive exchange of information with prospects. “We found out about their requirements and pain points at first hand”, says Niermann. “We could then demonstrate them our tailor-made drive solutions for the automation industry.” Again, it has proven positive that the experts from the NORD specialist departments were also present.

With SPS, NORD finishes a very successful trade fair year 2023. The first trade fair in 2024 will be the LogiMAT intralogistics trade fair from 19 to 21 March in Stuttgart.