Service
Frequently Asked Questions
Gear Unit
Check the oil fill level
Replace the seal
Contact Getriebebau NORD
- Check oil fill level
- Check the installation position for the version
- Check for overload
- Contact Getriebebau NORD
- Check the oil fill level
- Check the oil condition (oil analysis)
- Change the oil
- Check the gear unit fastening/foundation
- Contact Getriebebau NORD
- Check the gear unit fastening/foundation
- Check the coupling if fitted
- For frequency inverter operation, check the parameters
- Contact Getriebebau NORD
- The oil type and quantity are stated on the type plate
- The oil type and quantity are stated on the order confirmation
- Contact Getriebebau NORD
- Contact Getriebebau NORD
- Swap two phases on the electric motor (Notice! Not possible with back stop option!)
- Please contact Getriebebau NORD in case of back stop option
- Check the coupling if fitted
- Contact Getriebebau NORD
- Investigate the use of a frequency inverter
- Change the gearing
- Use a motor with a different number of pole pairs
- Contact Getriebebau NORD
Motor
- Check the parameter settings in case of frequency inverter operation
- Check the motor bearings and replace as necessary
- Check the fan/fan cover
- Contact Getriebebau NORD
- Check the parameter settings in case of frequency inverter operation
- Check the motor bearings and replace as necessary
- Check the motor mounting and modify as necessary
- If a coupling is fitted between the motor and the gear unit, check the alignment and the coupling
- Contact Getriebebau NORD
- Check the motor connection on the terminal board
- Check the supply voltage and the control of the protective device
- In the case of a brake motor, check the brake
- In the case of a back stop option, check the direction of rotation
- Contact Getriebebau NORD
- In the case of a brake motor, check the brake
- Check the application with regard to heavy starting / design
- Contact Getriebebau NORD
- Check the motor control or wiring
- If possible, operate the motor in the delta circuit; if necessary check or adapt the design with regard to overload
- Contact Getriebebau NORD
- If the drive does not have a back stop, swap two phases of the power supply
- Contact Getriebebau NORD
- Check the motor power supply
- Check the motor connection
- Check the application for excess load
- In the case of a brake motor, check the brake function
- Contact Getriebebau NORD
- Check the power supply
- Check the fuse / motor protector
- Check the design and modify as necessary
- Check the motor windings
- Contact Getriebebau NORD
- Check the fan
- For frequency inverter operation, check the minimum frequency/speed. Install an external fan if necessary
- Check the switching frequency for the operating mode of the motor and change the design as necessary
- Check the design and change the required motor power as necessary
- In the case of a brake motor, check the brake
- Check the installation location with regard to cooling
- Contact Getriebebau NORD
- Measure the contact resistance of the temperature monitor in the motor terminal box
- Contact Getriebebau NORD
- Measure the resistance at the contact of the temperature monitor in the motor terminal box
- Contact Getriebebau NORD
- Check the supply voltage to the brake
- If the brake is controlled by a rectifier, check the rectifier
- Measure the resistance of the brake coil
- Check the air gap of the brake
- Contact Getriebebau NORD
Frequency inverters, motor starters and field distributors
- Check the mains voltage and if necessary the control voltage (depending on the frequency inverter type).
- If necessary return the frequency inverter to the manufacturer for testing.
- Determine the cause of the switch on block via parameter (P700[3]) and the manual.
- Set automatic starting in P428 to "On", note the information in the manual.
- Check the motor data and match them with those on the type plate as necessary.
- Check the motor and the motor cable.
- Reduce the load.
- Check the precise error message via P700[1] and use the further remedial measures in the manual.
- If necessary return the frequency inverter to the manufacturer for testing.
- Check the load and speed, if necessary allow the motor to cool down or use an external fan.
- Check the thermistor resistance (TF≈200Ω/20C) and the connection.
- Bridge the thermistor input if it is not used.
- Increase the ramp time in P103.
- Use the V/f characteristic curve by setting parameters P211/212 to 0%.
- Use a suitable brake resistor.
- If necessary, adapt P217 (e.g. 200%).
- Determine the error code from the flashing code of the DS LED or read it out from P700. Then determine the suitable remedial measure from the manual.