Energy efficiency: How drive technology helps to reduce energy costs

According to studies, the consumption of electric drives amounts to up to 70 percent of the entire energy consumption in industry. This is not only a significant cost factor – it also provides a huge optimisation and savings potential. NORD DRIVESYSTEMS helps its customers to use this potential.

For example, NORD delivers up to 10,000 drive systems per project for varying intralogistics and baggage handling systems. Geared motors for the lower power range of up to 5.5 kW do not have a particularly high energy consumption themselves and the accumulating acquisition costs are also on a moderate level. However, if you consider the drives’ operating hours as well as the accumulating life cycle costs, high energy and business saving potentials present themselves. Such a drive running in intralogistics systems is usually in operations consisting of one to three shifts. If you take an installation performance of approx. 0.75 kW as a basis, then a single drive system roughly represents the electrical energy needs of a single-family home. The electricity consumption for the conveyor technology of a complete intralogistics or baggage handling system thus quickly reaches the dimension of a whole company. Considering we are desperately looking for solutions to reduce CO<sub>2</sub> emission, the following becomes clear: We need to act. Making use of this savings potential is sensible both in terms of climate policy and business management.

Recognising cost drivers and acting on it

The visible costs, that is the investment costs of a drive system, only amount to 15 percent of the life cycle costs. 85 percent of costs are incurred during the later operation: Energy costs, administrative costs, service and maintenance costs, training and documentation, personnel costs, spare part stocking as well as failures and downtimes. In times of climate change, the sustainability of the overall project is an important aspect of the public image. Acting in a sustainable manner will always have a positive impact on life cycle costs in times of rising prices for raw material and energy. What can operators of an intralogistics system do? For new systems, they should consider aspects like sustainability and life cycle costs accordingly in the tender criteria. For existing systems, an energy audit is recommended, which will show starting points for specific optimisations. The best results in drive design for the operator are made possible only by an intensive examination of the project and its requirements as well as a careful consideration of all economic aspects. NORD application engineers therefore support their customers with comprehensive analysis and consulting services right from the planning stage.

Load
[%]
IE3 asynchronous motor
[W]
IE5+ synchronous motor
[W]
DuoDrive (SK EVO 80)
[W]
100 (full load) 536 458 442
75 527 446 428
50 507 410 391
0 (idling) 462 336 318

Efficiency and costs balanced perfectly

The new IE5+ motor generation from NORD DRIVESYSTEMS has been designed with a focus on use in the intralogistics sector. The especially compact and energy-efficient synchronous motors feature a high efficiency over a wide torque range and thus also optimum energy consumption performance in partial load and partial speed ranges. A comparison of a conventional IE3 asynchronous motor (0.75 kW, 83% motor efficiency, bevel gear unit) with a corresponding IE5+ synchronous motor (0.75 kW, 93% motor efficiency, bevel gear unit) show energy savings of about 11% with 16 operating hours per day (4000 p.a.) and a CO<sub>2</sub> emission factor of 366 g/kWh. This corresponds to 400  kWh and 0.15  t  CO<sub>2</sub> p.a.

Due to an efficient use of materials and a compact size, the IE5+ synchronous motor has a weight advantage of more than 50% compared to IE3 asynchronous motors within the same power range. NORD DRIVESYSTEMS delivers IE5+ synchronous motors with a motor efficiency of up to 95% for the power range of 0.35 to 4.0 kW and in TENV as well as TEFC designs.

Power
[kW]
IE5+ IE3 Installation space
IE5 < IE3
Weight
IE5 < IE3
0.5 71 F1/8  80 SP/4  -31.7%  -27.8% 
1.0 71 F2/8  90 SP/4  -54.1%  -50.3% 
1.5 71 F3/8  90 LP/4  -54.1%  -52.4% 
2.2 71 F4/8  100 LP/4  -58.8%  -61.2% 
3.0 90 F3/8  100 AP/4  -32.1%  -49.6% 
3.7 90 F4/8  112 MP/4  -53.1%  -56.1% 

Additional sustainability impacts

Additionally, less volume and less weight result in reduced transport costs and are therefore more environmentally sound. The mentioned 0.75 kW motor weighs about 10 kg in the IE3 version, the comparable IE5+ motor only weighs about 6 kg. If a IE5+ motor is delivered from Hamburg to Stuttgart instead of an IE3 motor, the CO<sub>2</sub> emissions are reduced by about 120 g per motor. Considering the sketched-out size of the system with up to 10,000 drives and the fact that drive systems from NORD DRIVESYSTEMS are delivered around the globe, this demonstrates that the motors belonging to the range of high efficiency products not only contribute directly to sustainability by reducing energy consumption but also indirectly, thanks to their smaller volume and weight.

The next step: Two become one

Speed
(Operating point)
Load
(Operating point)
IE2 GM asynchronous  IE3 GM asynchronous  DuoDrive IE2 vs. DuoDrive 
(Savings)
IE3 vs. DuoDrive
(Savings)
75 % 25 % 64.4% 68.6% 87.5% -23.1% -18.9%
50 % 25 % 64.2% 68.2% 88.2% -24.0% - 20.0%
50 % 50 % 73.6% 76.4% 91.5% -17.9% -15.1%

How a field distribution system is built: A look behind the scenes in Aurich

The age of industrial mass production with only a few product versions and large quantities is long gone. Individuality is in greater demand than ever. Customers increasingly demand specific configurations which are precisely tailored to their individual requirements. This megatrend will continue in the future. At the same time, even smaller batches are required. Conventional factory structures cannot cope with this increasing variance with reducing batch sizes. An intelligent, variable and efficient production procedure is necessary to be able to respond quickly and flexibly to customer requirements and changes in the market. Industry 4.0, smart, fully networked production provides the answer to this.

Energy efficiency classes: Current regulations and upcoming changes

In this post, we want to advise you about energy efficiency regulations in drive technology. As expected, the whole matter is very complicated, and many details and special cases must be observed, so that we can only go into a few general points here. The currently applicable energy efficiency regulations for all countries worldwide can be found up-to-date on our dedicated efficiency regulations website . Our NORD contact partners will, of course, also be glad to provide you with information on the regulations applicable to your project.

NORDAC ON / ON+ SK 300P

  • Power: 0.5 - 5.0 hp (0.37–3.7 kW)
  • Protection Class: IP55, IP66
  • Wall or motor mounting
  • Simple integration via multi-protocol ethernet interface
  • Fast plug-and-play commissioning
Back to overview